Skip to main content
Associate III
Jun 10, 2025 3:33 PM UTC
Question

Multicast Downlinks Queued but Not Reaching End Devices

Hi everyone,

I'm experiencing an issue with multicast group communication in my LoRaWAN setup. I have created a multicast group and am attempting to send downlinks to my end devices (STM32 B-L072Z-LRWAN1). The downlinks are getting queued and sent to the gateway, but they never seem to reach the end devices.

Here is the part of my code responsible for sending the multicast downlinks:

def send_downlink():
now = datetime.now().strftime('%Y-%m-%d %H:%M:%S')
print(f"[{now}] Sending downlink to multicast group (Port: {FPORT}, Payload: {PAYLOAD_HEX})...")

try:
channel = grpc.insecure_channel(GRPC_SERVER)
client = api.MulticastGroupServiceStub(channel)
auth_token = [("authorization", f"Bearer {API_TOKEN}")]
payload_bytes = bytes.fromhex(PAYLOAD_HEX)

req = api.EnqueueMulticastGroupQueueItemRequest()
req.queue_item.f_port = FPORT
req.queue_item.data = payload_bytes
req.queue_item.multicast_group_id = MULTICAST_GROUP_ID

# Send request
start_time = time.time()
resp = client.Enqueue(req, metadata=auth_token)

# Check for valid response
if resp.f_cnt > 0:
print(f"Downlink queued successfully! Frame Counter: {resp.f_cnt}")
return True
else:
print("Downlink queued but with no valid frame counter")
return False

except grpc.RpcError as e:
status_code = e.code()
details = e.details()
print(f"gRPC Error ({status_code.name}): {details}")

if status_code == grpc.StatusCode.UNAUTHENTICATED:
print("ERROR: Invalid or expired API token")
elif status_code == grpc.StatusCode.NOT_FOUND:
print("ERROR: Multicast group not found")
return False

except Exception as e:
print(f"General error: {str(e)}")
return False



I have configured the multicast group keys on the end devices as follows:

#if (LORAMAC_MAX_MC_CTX == 1)
#define SESSION_MC_KEYS_LIST \
{ \
.KeyID = MC_KEY_0, \
.KeyValue = { 0x8d, 0x29, 0xc7, 0x0c, 0xd7, 0x10, 0x42, 0xca, 0xa9, 0xd2, 0x79, 0xe0, 0x8d, 0xb3, 0x94, 0xe2 }, \
}, \
{ \
.KeyID = MC_APP_S_KEY_0, \
.KeyValue = { 0x5d, 0xda, 0x93, 0xc3, 0xbf, 0x26, 0xc8, 0x2b, 0xe4, 0x6e, 0xbc, 0x54, 0xe6, 0x87, 0xd3, 0x0d }, \
}, \
{ \
.KeyID = MC_NWK_S_KEY_0, \
.KeyValue = { 0xfc, 0xc2, 0x36, 0x34, 0xb1, 0xa3, 0xc7, 0x50, 0xd3, 0xde, 0x68, 0xc1, 0xb8, 0xe9, 0x9a, 0xb4 }, \
},
#else /* LORAMAC_MAX_MC_CTX > 1 */
#define SESSION_MC_KEYS_LIST \
{ \
.KeyID = MC_KEY_0, \
.KeyValue = { 0x8d, 0x29, 0xc7, 0x0c, 0xd7, 0x10, 0x42, 0xca, 0xa9, 0xd2, 0x79, 0xe0, 0x8d, 0xb3, 0x94, 0xe2 }, \
}, \
{ \
.KeyID = MC_APP_S_KEY_0, \
.KeyValue = { 0x5d, 0xda, 0x93, 0xc3, 0xbf, 0x26, 0xc8, 0x2b, 0xe4, 0x6e, 0xbc, 0x54, 0xe6, 0x87, 0xd3, 0x0d }, \
}, \
{ \
.KeyID = MC_NWK_S_KEY_0, \
.KeyValue = { 0xfc, 0xc2, 0x36, 0x34, 0xb1, 0xa3, 0xc7, 0x50, 0xd3, 0xde, 0x68, 0xc1, 0xb8, 0xe9, 0x9a, 0xb4 }, \
},
#endif /* LORAMAC_MAX_MC_CTX */


Despite the downlinks being queued and sent to the gateway, they are not reaching the end devices. Has anyone encountered a similar issue or have any suggestions on what might be going wrong?

Thanks in advance for your help!

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Jun 12, 2025 9:45 AM UTC

Hello @Mariiian09 

This seems to be related to the LoRaWAN server you are using. So, i suggest you contact them for more help.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.