Skip to main content
Senior
Sep 6, 2024 2:31 AM UTC
Question

Mouse report descriptor from nRF52 NORDIC gives driver error on STM32wb55!

Why this mouse report descriptor is working on nRF52 Nordic Semiconductor hardware and give driver error after BLE HID Bluetooth connection on STM32wb55?

[Keyboard report descriptor from nRF52 is working OK].

Report Descriptor should be not dependent from hardware!

// FROM nRF52 NORDIC - ble_hid_mouse_pca10040_s132 example:

static uint8_t report_mouse[] = {
0x05, 0x01, // Usage Page (Generic Desktop)
0x09, 0x02, // Usage (Mouse)
0xA1, 0x01, // Collection (Application)

// Report ID 1: Mouse buttons + scroll/pan
0x85, 0x01, // Report Id 1
0x09, 0x01, // Usage (Pointer)
0xA1, 0x00, // Collection (Physical)
0x95, 0x05, // Report Count (3)
0x75, 0x01, // Report Size (1)
0x05, 0x09, // Usage Page (Buttons)
0x19, 0x01, // Usage Minimum (01)
0x29, 0x05, // Usage Maximum (05)
0x15, 0x00, // Logical Minimum (0)
0x25, 0x01, // Logical Maximum (1)
0x81, 0x02, // Input (Data, Variable, Absolute)
0x95, 0x01, // Report Count (1)
0x75, 0x03, // Report Size (3)
0x81, 0x01, // Input (Constant) for padding
0x75, 0x08, // Report Size (8)
0x95, 0x01, // Report Count (1)
0x05, 0x01, // Usage Page (Generic Desktop)
0x09, 0x38, // Usage (Wheel)
0x15, 0x81, // Logical Minimum (-127)
0x25, 0x7F, // Logical Maximum (127)
0x81, 0x06, // Input (Data, Variable, Relative)
0x05, 0x0C, // Usage Page (Consumer)
0x0A, 0x38, 0x02, // Usage (AC Pan)
0x95, 0x01, // Report Count (1)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0xC0, // End Collection (Physical)

// Report ID 2: Mouse motion
0x85, 0x02, // Report Id 2
0x09, 0x01, // Usage (Pointer)
0xA1, 0x00, // Collection (Physical)
0x75, 0x0C, // Report Size (12)
0x95, 0x02, // Report Count (2)
0x05, 0x01, // Usage Page (Generic Desktop)
0x09, 0x30, // Usage (X)
0x09, 0x31, // Usage (Y)
0x16, 0x01, 0xF8, // Logical maximum (2047)
0x26, 0xFF, 0x07, // Logical minimum (-2047)
0x81, 0x06, // Input (Data, Variable, Relative)
0xC0, // End Collection (Physical)
0xC0, // End Collection (Application)

// Report ID 3: Advanced buttons
0x05, 0x0C, // Usage Page (Consumer)
0x09, 0x01, // Usage (Consumer Control)
0xA1, 0x01, // Collection (Application)
0x85, 0x03, // Report Id (3)
0x15, 0x00, // Logical minimum (0)
0x25, 0x01, // Logical maximum (1)
0x75, 0x01, // Report Size (1)
0x95, 0x01, // Report Count (1)

0x09, 0xCD, // Usage (Play/Pause)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x0A, 0x83, 0x01, // Usage (AL Consumer Control Configuration)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x09, 0xB5, // Usage (Scan Next Track)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x09, 0xB6, // Usage (Scan Previous Track)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)

0x09, 0xEA, // Usage (Volume Down)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x09, 0xE9, // Usage (Volume Up)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x0A, 0x25, 0x02, // Usage (AC Forward)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0x0A, 0x24, 0x02, // Usage (AC Back)
0x81, 0x06, // Input (Data,Value,Relative,Bit Field)
0xC0 // End Collection
};

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 20, 2024 6:06 PM UTC

Hello @GS2 

Could you please follow the recommendations on the answer of this post. I think your use case need direct contact.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.