Skip to main content
This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 17, 2025 5:22 PM UTC

Hello @nima.askari 

I've personally generated a code on the STM32WB using the STM32_WPAN and the P2P server application type. After compilation, everything works fine and no need to add the file manually (using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1). If you have the need to use the ble_types.h and it is not included, you need to ad it manually.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Andrew Neil
Super User
Jun 17, 2025 12:28 PM UTC

Is that a question, or a statement?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 17, 2025 5:22 PM UTC

Hello @nima.askari 

I've personally generated a code on the STM32WB using the STM32_WPAN and the P2P server application type. After compilation, everything works fine and no need to add the file manually (using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1). If you have the need to use the ble_types.h and it is not included, you need to ad it manually.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.