Skip to main content
LaoMa
Associate III
Jul 15, 2021 1:46 AM UTC
Question

Migration from st32f1 to stm32wb

Hi,

into the SMT32CubeIDE is it possible to migrate code from STM32F1xx to ST32WB families?

I mean, using the same basic code of the F103 and adding the BLE of the WB family?

Thanks for any reply

Maurizio

PS: in case, is there any migration app note?

This topic has been closed for replies.

3 replies

Remi QUINTIN
ST Technical Moderator
Jul 16, 2021 2:20 PM UTC

I don’t think porting your application developed for an STM32F1 device will work as is on the STM32WB. The HAL should hide the low level differences but there are still some adaptation to perform. But in the end it is not impossible.

Your application would run on the M4 core only.

Tesla DeLorean
Guru
Jul 16, 2021 3:22 PM UTC

Generally speaking the most efficient ways to port between STM32 families is to create a shell or donor project on the target platform, get that working and the plumbing for some diagnostic output, and hard fault / error handlers, and then use a merge tool to pull over selective portions which you can test and validate.

How complex the process is depends on how cleanly you've used the HAL abstraction

There are frequently not tutorials/app-notes because ST doesn't have a lot of real-world applications, and you need to have ported a couple of things of to have a real appreciation of the process in complex situations.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LaoMa
LaoMaAuthor
Associate III
Jul 19, 2021 3:25 AM UTC

Thanks for replies,

It was just a question to know if exist a direct process to change the STM32 in a project.

My code is not complex, it has been ported by a Keil project into STM32CubeIDE and fully adapted at the HAL libraries.

I think that the suggestion to create a new project with the WB MCU and copy the other general SW a few at time it's the only real chance to do this!

Bye bye