Migrating from STM32WL55JC17 (UFBGA) to STM32WL55CC (UFQFPN) – Missing Pin Equivalents
- 2 replies
- 543 views
Hello STM32 Community,
I'm working on a custom board based on the MB1389 (Nucleo-WL55JC) reference design, which uses the STM32WL55JC17 (UFBGA) package. Now, I am migrating to the STM32WL55CC in the UFQFPN package for cost and space reasons.
While adapting the schematic, I noticed the following pins from the original design are not available in the UFQFPN package:
PC3
PC4
PC5
PB14
PB1
VSSRF
VREF+
I understand that the pin count is reduced in the UFQFPN package, but I need guidance on the following:
Are there any internal remapping or alternative GPIOs for the above functions in the STM32WL55CC UFQFPN package?
How should I handle VSSRF and VREF+, since they are critical for RF and analog operations? Can they be connected internally, or do they need external routing?
Any advice or reference designs (for UFQFPN-based layouts) that clarify how to proceed with features that originally used those missing pins?
For reference, I am attaching a snippet of my schematic based on MB1389, where these pins are currently used.