Question
MCU STM32WLE5 radio wake-up reason
Hi,
For my project I need to put a MCU STM32WLE5CCU6 in standby mode and configure several wake-up type :
- Wake-up pin 1 on PA0
- RTC wake-up
- Radio wake-up on a LoRa message received by the embedded Sub-GHz radio module of the MCU with the bit EWRFIRQ (reg: PWR_CR3)
I can recognize the wake-up from :
- the pin PA0 with WUF1 (reg: PWR_SR1)
- the RTC with WUFI (reg: PWR_SR1)
However, I can't find a solution to check that the MCU have been waked-up by the Sub-GHz radio module.
Do you have a solution ?
Other fact, every time the MCU is waked-up whichever the reason, the bit WUF1 is set when the wake-up on pin 1 is configured. Is it a bug ?
Note : I reinitialize the flag of the wake-up pin 1 reason before putting the MCU in standby mode.
Thanks in advance
MaxB1000ien