Skip to main content
KHoll
Visitor II
Apr 2, 2020 3:33 PM UTC
Question

Max output power when operating at 1.8V?

To achieve the +6dBm output power on the WB55, VDD needs to be > 1.95V. What is the max ouput power you can achieve if the device is operated at 1.8V?

This topic has been closed for replies.

1 reply

Remi QUINTIN
ST Technical Moderator
Apr 3, 2020 7:55 AM UTC

With SMPS ON,  it is required to have VDD > 1V95 to get Pmax = 6dBm.

But with SMPS BYPASS, Pmax = 6 dBm can be achieved with only VDD > 1V71.

We did not test the configuration you ask for: SMPS ON with VDD = 1V8.