Skip to main content
DPrie.1
Associate II
Mar 4, 2022 1:47 PM UTC
Question

LoRaWAN Session keys store is already working on V2.1.0 ?

Hello everybody,

I'm using the AT code modified in order to join my own server with an OTAA configuration in a solar application, so every morning the system goes up, and late afternoon the system shuts down.

I want to store session keys, counters and all stuff necesary for not rejoining server each time a power down/up is done.

CONTEXT_MANAGEMENT_ENABLED is defined to 1, and I needed to add some libraries related to nvm (NvmDataMgmt.c/.h and nvmm.c/.h).

When firmware enters in LmHandlerConfigure(), I receive a "Restored", showing that we are here:

 // Restore data if required
 nbNvmData = NvmDataMgmtRestore( );
 
 // Try to restore from NVM and query the mac if possible.
 if( nbNvmData > 0 )
 {
 	MW_LOG(TS_OFF, VLEVEL_M, "###### RESTORED\r\n");
 CtxRestoreDone = true;
 }
 else
 {
 	MW_LOG(TS_OFF, VLEVEL_M, "###### NOT RESTORED\r\n");
 CtxRestoreDone = false;
 }

However, I try to send a message without doing a AT_JOIN and always returns AT_BUSY.

Need to send some special AT command before start sending messages? Or maybe the keys are not restored correctly?

Thank you very much!

Regards,

This topic has been closed for replies.