LoRaWAN Project using P-Nucleo-LRWAN2
- 3 replies
- 1885 views
I am using P-NUCLEO-LRWAN2 package, and Nucleo STM32 L476RG as my end node.
The end node is configured as :
Region and Frequency plan: EU863-870
Data is transmitted at: TX on freq 868100000 Hz at DR 0, TX on freq 868500000 Hz at DR 0, TX on freq 868300000 Hz at DR 0
Device EUI Is used as is generated by the MCU. AppEUI is 01:01:01:01:01:01:01:01 and AppKey: 2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3C.... and it is registered on the TTN network on which it has the frequency plan as:
Europe 863-870 MHz (SF12 for RX2).
here is how gateway is configured:
Device EUI: as mentioned on the package
Region / Frequency Plan :
Europe 863-870 MHz (SF12 for RX2)
Also the Gateway status is Connected.
"No activity yet" message is displayed on the end node. Even The end device is not detected as an activity. But the Controller is sending the dummy data. joined failed message is visible on terminal through Com port. What can be the issue? why the device is not seen by the network server? Even on Loriot Gateway is configured correctly and is connected. but the end not status is: Never Seen. any help in this regard will be grateful. Thank you