Skip to main content
IKarg.1
Associate II
Jul 16, 2022 2:06 PM UTC
Solved

LoRaWAN is locked when I try to start a new project with stm32wl MCU. What peripherals are required to enable it or to make LoRa work?

Hello,

When I try to start a new project with stm32wl MCU, I see that LoRaWAN is locked in cubeMX. When I import one pre-configured project, I see that it is enabled, but I don't know if I have to enable some other peripherals first to enable LoRaWAN and configure it. Can someone help me understand this problem here?

Bests,

Isaac

This topic has been closed for replies.
Petr DAVID
Petr DAVIDBest answer
ST Employee
Jul 20, 2022 2:27 PM UTC

Hello IKarg.1,

the LORAWAN middleware can be enabled only when SUBGhz IP is activated and for dual core project you need to also activate the IPCC. This note should also be shown in the STM32CubeMX when you click on the lock LORAWAN category. For correct setting I would recommend you to check the example projects. You can also find useful online course available here.

Best regards,

Petr

3 replies

Petr DAVID
Petr DAVIDBest answer
ST Employee
Jul 20, 2022 2:27 PM UTC

Hello IKarg.1,

the LORAWAN middleware can be enabled only when SUBGhz IP is activated and for dual core project you need to also activate the IPCC. This note should also be shown in the STM32CubeMX when you click on the lock LORAWAN category. For correct setting I would recommend you to check the example projects. You can also find useful online course available here.

Best regards,

Petr

New.Fish
Associate III
Sep 12, 2022 8:44 AM UTC

Hi Peter,

In "LoRaWAN commiddioning" , where is the "se-identity" parameters (key) from? from the IC memory?

Regards

Sam

IKarg.1
IKarg.1Author
Associate II
Jul 27, 2022 2:34 PM UTC

Thank you Petr for the help.