Skip to main content
OGarc.1
Associate
Feb 11, 2022 9:07 AM UTC
Solved

LoRaWAN integration in STM32WB55

I am using the STM32WB55 microcontroller where I use BLE and integrate my main program with code that I am implementing.

On the other hand, I need to use LoRaWAN and for this I use the HOPERF RFM95 module in which only the radio part is integrated but in which I could integrate the MAC layer in the STM32WB55 to be able to use LoRaWAN. 

Is it possible to integrate the MAC layer code inside my STM32WB55 or is it better to use a LoRaWAN module like the CMWX1ZZABZ and control it by AT commands?

Regards,

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 9, 2022 4:36 PM UTC

Hello,

I think is better to use a LoraWAN module and control it by AT commands. You can look STEVAL-ASTRA1B board which embed the STM32WB5MMG module and the STM32WL55JC SoC:

https://www.stmicroelectronics.com.cn/en/evaluation-tools/steval-astra1b.html#overview

Best Regards

3 replies

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 9, 2022 4:36 PM UTC

Hello,

I think is better to use a LoraWAN module and control it by AT commands. You can look STEVAL-ASTRA1B board which embed the STM32WB5MMG module and the STM32WL55JC SoC:

https://www.stmicroelectronics.com.cn/en/evaluation-tools/steval-astra1b.html#overview

Best Regards

Julien NGUYEN
ST Employee
Jun 24, 2022 7:30 AM UTC

Hi Remy,

Reading the data brief of the product I found some sensors are already built-in

0693W00000NsgQpQAJ.pngBut I need to add a Time of Flight distance sensor to make a POC. It is I2C communication sensor. Do you know if it is possible to add an external I2C sensor? Or do you have other similar solution ?

Thanks,

Julien

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Remy ISSALYS
ST Technical Moderator
Jun 28, 2022 2:02 PM UTC

Hi,

Yes, you can add an external I2C sensor through expansion connector, see part 1.4.2.9 of UM2966.

Best Regards