Skip to main content
Visitor II
Dec 11, 2024 2:42 PM UTC
Question

LoRaWAN FUOTA class C

Hey everybody,

I am currently working on a project which involves a firmware update over the air (using the nucleo wl55jc1 board). i have found an example project through the official website (https://www.st.com/en/embedded-software/stm32cubewl.html) and unzipped the file directly onto my c disk and use powershell to execute the scripts. at first i tried the code without changes besides the changes in the se-identity.h file and everything worked fine see the picture below for the ouptut on the serial monitor.

working_classAworking_classA

once i concluded the project worked i tried to change the class from A to C and got the following

IdiotStudent_0-1733927114845.png

i expected to still see the tx sending data. however that just stopped. i did a deep dive into the code but that just got me more confused. its getting me nowhere and i am not sure on how to proceed. i hope you fine people may shine some light on it. i am using chirpstack as networkserver.

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Jan 7, 2025 11:24 AM UTC

Hello @IdiotStudent 

It may be an issue on the gateway side. Are you sure is not that?

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Mar 24, 2025 11:18 AM UTC

Hii, 

 

I also made the same changes and flashed the end node but my program gets stuck on KMS_init function 

 

Could you provide some guidance on this ?

 

Reagrds, 

Suyash