Skip to main content
Associate
Jul 7, 2025 7:11 AM UTC
Solved

LoRaWAN cubemx generated code is showing error

../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'

1650 | ( MacCtx.McpsIndication.ResponseTimeout > 0 ) )

| ^ The above error is occuring every time ,  if i remove this then adc_if.c is not found error occurs and I don't want to include the adc_if.c file in my code

This topic has been closed for replies.
Dana Myers
Dana MyersBest answer
Senior
Jul 7, 2025 3:50 PM UTC

See my comment; 1.3.1 conditionally includes ResponseTime for LoRaWAN Link Layer 1.0.4 and 1.1.1 (see LoRaMacInterfaces.h around line 1518), but LoRaMac.c unconditionally accesses it, regardless of LoRaWAN Link Layer version.

I humbly suggest firmware changes are tested with 1.0.3 and 1.0.4 both, that would have caught this.

5 replies

ST Technical Moderator
Jul 7, 2025 8:23 AM UTC

Hello @avinashkumar 

Could you please provide your ioc in order to investigate the issue?

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
Jul 7, 2025 9:55 AM UTC

check now .ioc file 

if any problem in this do let me know

Dana Myers
Senior
Jul 7, 2025 3:46 PM UTC

This is a bug in the STM32WL FW 1.3.1 package. The following code at line 1518 in LoRaMacInterfaces.h appears to have been added in 1.3.1 and conditionally includes the ResponseTimeout item if LoRaWAN Link Layer is 1.0.4 in CubeMX.

If you select LoRaWAN Link Layer version 1.0.3, the ResponseTimeout item is not included and the error occurs.

This needs to be corrected by ST in the FW package. A possible work-around is to comment-out the #if/#endif in the code snippet so ResponseTimeout is always included regardless of LoRaWAN Link Layer which should be harmless; if you do this, you will need to re-do it every time CubeMX generates code and over-writes the change.

 
 bool DeviceTimeAnsReceived;
#if (defined( LORAMAC_VERSION ) && (( LORAMAC_VERSION == 0x01000400 ) || ( LORAMAC_VERSION == 0x01010100 )))
 /*!
 * Response timeout for a class b or c device when a
 * confirmed downlink has been received. In all other
 * cases this variable is 0.
 */
 TimerTime_t ResponseTimeout;
#endif /* LORAMAC_VERSION */
}McpsIndication_t;

 

STTwo-32
ST Technical Moderator
Aug 5, 2025 12:54 PM UTC

Hello @avinashkumar @Dana Myers 

This behavior has been reported internally for correction (under internal ticket number 215349). Thank you so much for the details.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.