LoraMac. Only three chanels - how to make more?
Hi everyone!
I have stm32L072 chip and sx1272 lorachip.
I had developed a simple end-node device with stm32 lrwan library and endnode example for nucleo board.
Developed by Atollic True Studio.
Versions is: MAC_VERSION= 04.04.02.00 and STM32CubeExpansion_LRWAN_V1.3.1
options that i had used to:
1)LORAWAN_ADR_ON - true;
2)Global define REGION_EU868;
3)server's chanels list:
3.1) FIXED; (servers chanel default);
3.2) FIXED;
3.3) FIXED;
3.4) 867,1 MHz;
3.5) 867,3 MHz;
3.6) 867,5 MHz;
3.7) 867,7 MHz;
3.8) 867,9 MHz;
Questions:
My firmware program is always send data by three chanels: 868,1MHz, 868,3MHz, 868,3MHz. How can I add the missing channels?