Skip to main content
Pavel_47
Associate III
May 8, 2025 4:08 PM UTC
Solved

Looking for eval/dev/NUCLEO board allowing to program/debug custom board

Hello,

I'm looking for a board that provides all program/debug signal on a header while allowing to disconnect on-board MCU.

I've looked at a few NUCLEO boards - only JTCK, JTMS, NRST, SWO are exposed to a header (with possibility to disconnect on-board MCU using jumpers and solder bridges), but not MCO, STLK_TX and STLK_RX.

Does exist a board that exposes whole this stuff ?

Thanks.

Pavel.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 8, 2025 5:29 PM UTC

You may refer to this FAQ: How to program an STM32 using the on-board ST-LINK... - STMicroelectronics Community and use the JP5.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

STTwo-32
ST Technical Moderator
May 8, 2025 4:43 PM UTC

Hello @Pavel_47 

I may suggest you the Nucleo-68 board of the P-NUCLEO-WB55, it provide GND, NRST, SWDIO, SWCLK, SWO, TX_STlink (VCP) and TX_STlink (RCP) on the JP5:

STTwo32_0-1746722582677.png

For the MCO, I don't know if there is a board with STLINK MCO is provided on a header.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel_47
Pavel_47Author
Associate III
May 8, 2025 5:25 PM UTC

Hello @STTwo-32,

Thanks ! A couple of additional questions nevertheless:

The required signals are exposed on two headers: CN13 and CN14. But surprisingly SWO isn't exposed. Any reason for that ?

Pavel_47_0-1746724913107.png

Moreover on another document (mb1355-wb55rg-d01_schematic.pdf) there are not at all CN13, CN14. What does it mean ?

Pavel_47_1-1746725027632.png

Sincerely,

Pavel.

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 8, 2025 5:29 PM UTC

You may refer to this FAQ: How to program an STM32 using the on-board ST-LINK... - STMicroelectronics Community and use the JP5.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
May 8, 2025 5:24 PM UTC

I'm guessing by "MCO" you mean the ~8 MHz signal coming from ST-Link. FWIW, this isn't required for debugging and doesn't appear on any standard programming header.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel_47
Pavel_47Author
Associate III
May 8, 2025 5:28 PM UTC

@TDK I asked IA for this signal. It says that any critical signal can be exposed to this pin. Anyway as you said it isn't critical