Skip to main content
Visitor II
Apr 21, 2024 2:05 PM UTC
Solved

learning lrwan1

hello im doing a school project using a Nucleo-F411RE with a I-NUCLEO-LRWAN1 expansion, anyone got a good text or video tutorial how i connect the two boards?

im using the stm32cubeide

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 21, 2024 2:51 PM UTC

Hello @JoaoFoonseca and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to refer to the Sub-Ghz Phy examples on the I-CUBE-LRWAN. I should be helpful to understand how it should work. For me, i suggest you to use our STM32 long range product the STM32WL that is an MCU with Sub-Ghz communication features. You can find on YouTube lot of videos that help you working with this product. Even a full STM32CubeWL library for this product. For more details refer to this link.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 21, 2024 2:51 PM UTC

Hello @JoaoFoonseca and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to refer to the Sub-Ghz Phy examples on the I-CUBE-LRWAN. I should be helpful to understand how it should work. For me, i suggest you to use our STM32 long range product the STM32WL that is an MCU with Sub-Ghz communication features. You can find on YouTube lot of videos that help you working with this product. Even a full STM32CubeWL library for this product. For more details refer to this link.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 22, 2024 10:57 AM UTC

@JoaoFoonseca wrote:

 a good text or video tutorial how i connect the two boards?


What do you mean by that?

Connecting the boards is easy - the  I-NUCLEO-LRWAN1 just plugs into the Adruino sockets of the Nucleo-F411RE.

Note that the  I-NUCLEO-LRWAN1 is now classed as Obsolete.

EDIT:

The catch here is that the UART TX & RX on the Arduino D1 & D0 pins is needed for the communication between the Nucleo processor and the USI module on the shield.

Therefore SB13 & SB14 will need to be removed - and this means that you won't have any comms over the ST-Link's Virtual COM Port (VCP).

As @STTwo-32 said, you may be better off with an STM32WL board - or, perhaps the B-L072Z-LRWAN1...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.