Skip to main content
Associate III
Apr 12, 2026 2:44 PM UTC
Question

Joining a LoRaWAN network only once

Can I join a LoRaWAN network only once?
so that after a software or hardware reset, i would not need to join the same network once again

I am working with LoRaWAN_End_Node_LBM example

3 replies

ST Technical Moderator
Apr 13, 2026 8:37 AM UTC

Hello @onass ,

I think through defining the CONTEXT_MANAGEMENT_ENABLED option, which allows the device to store and restore its LoRaWAN stack context (including session and network information) across resets.

More details of this feature in the AN5406, Section 15. LoRaWAN context management description.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
onassAuthor
Associate III
Apr 14, 2026 3:11 PM UTC

Hello @Imen.D ,

I am using LoRaWAN_End_node_LBM example in v1.5.0, which does not has CONTEXT_MANAGEMENT_ENABLED  option.

Associate
May 13, 2026 8:41 AM UTC

Hello,
Same problem here. Did you find a solution?

Thanks,

Pierre.