Question
It is possible to control multiple devices using multiple models in an element??
An element in a node supports multiple models . STM32Cube_FW_WB_V1.8.0 supports 20 models per node, but it only supports 3 elements per node.
I want to control more than 3 devices per node in my project.
If i disable MODEL BINDING, it is possible to control two devices using two models (Generic onoff server and light lightness server) in a single element??
I'm using STM32Cube_FW_WB_V1.8.0 package with STM32WB55 Nucleo Pack (STM32WB55RGV6 MCU) and ST BLE Mesh app.