Skip to main content
TSchl.1
Visitor II
Jan 31, 2020 1:44 PM UTC
Question

Issues with BLE_DataThroughput example project

I am trying to compile the BLE_DataThroughput example project. First, I started with CubeIDE. The program compiles for BLE central, but does not behave as expected on the hardware. For peripheral (#define CFG_BLE_CENTRAL 0) there are unknown symbols in the pre-compiler.

So I installed SW4STM32. Now both cases compile without error and #define CFG_BLE_CENTRAL 1 works as expected in hardware (output to the serial console, but does not find the other board to connect to).

However, #define CFG_BLE_CENTRAL 0 compiles as well, but does not output anything.

Do you have any hints on how to get started with the example project? Thank you very much!

This topic has been closed for replies.

1 reply

Remi QUINTIN
ST Technical Moderator
Feb 17, 2020 4:12 PM UTC

Using CubeWB FW delivery v1.4.0 with the SW4STM32 project and #define CFG_BLE_CENTRAL 0, all is OK on our side.

We can see the traces on the terminal.