Skip to main content
Visitor II
Nov 14, 2026 5:00 AM UTC
Question

Issues on the P-NUCLEO-STM32WB to upgrade the FUS version

I want to upgrade the FUS (at the moment it is FUS version 1.2.0) to upload next version 2.2.0, the FTD thread stack. But when I upload the stm32wb5x_FUS_fw.bin with SMT32CubeProgrammer, I got the following eror: "Error: FUS_AUTH_TAG_CUST_NOTFOUND".

 

1 reply

ST Technical Moderator
Nov 17, 2026 3:00 PM UTC

Hello ​@gayathrikolli  and welcome to the Community,

FUS_AUTH_TAG_CUST_NOTFOUND means the FUS did not found the required Customer Authentication tag in the downloaded image.

Make sure to use only the official stm32wb5x_FUS_fw.bin from the latest STM32CubeWB package. Use also the latest release of STM32CubeProgrammer.

Could you provide the values of the 2 option bytes SFSA and SBRV?

Check the following resources that may help you

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks