Skip to main content
Visitor II
Mar 17, 2026 9:16 AM UTC
Question

Issue Uploading New Firmware via OTA After Flashing Custom Firmware on STM32WB5MMG

I am working with the STM32WB5MMG and implementing firmware updates using OTA. For testing, I am using the ST BLE Sensor Android application.

What I Tested

I first tested OTA using the example projects available in the STM32CubeWB firmware package:

  • Heartrate_ota

  • P2PServer_ota

Both examples work correctly. I can:

  • Flash the example firmware

  • Connect using the ST BLE Sensor app

  • Upload another firmware via OTA successfully

My Custom Firmware

After verifying OTA with the examples, I created my own firmware that includes:

  • Custom BLE service

  • Custom characteristics

  • Custom UUIDs and device name

When I upload this custom firmware via OTA from the example firmware, the update completes successfully and the device runs my application correctly.

Problem

After my custom firmware starts running:

  • The device no longer appears in the ST BLE Sensor app as OTA-capable.

  • I cannot upload another firmware via OTA.

  • The device does not advertise as an OTA device like the Heartrate_ota or P2PServer_ota examples.

So OTA works only once (from the example firmware to my custom firmware), but subsequent OTA updates are not possible.

Question

How can I implement OTA functionality in a custom firmware application so that:

  • The device continues to be recognized as OTA-capable by the ST BLE Sensor app.

  • Multiple OTA updates can be performed.

  • My custom BLE services can coexist with OTA functionality.

Most documentation explains OTA using the existing examples, but I could not find guidance on integrating OTA into a new custom application.

Any documentation, references, or recommended procedure would be very helpful.

1 reply

ST Technical Moderator
Apr 9, 2026 3:03 PM UTC

Hello @Praveen4 ,

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks