Skip to main content
Selim Sagir
Associate III
Sep 14, 2020 1:50 PM UTC
Question

Is there a library using only for Lora not Lorawan?

Hi all,

I am looking for a library use with B-L072Z-LRWAN1 for Lora comm between two kits. Is there any library for this including only Lora libraries not Lorawan?

Thanks.

Selim.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Sep 14, 2020 4:59 PM UTC

The LRWAN libraries contain various layers, the PingPong examples only use the LoRa Radio functionality, without LoRaWAN

Look at the code supporting the SX1272 or SX1276

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Selim Sagir
Associate III
Sep 15, 2020 10:06 AM UTC

Yes I know ping pong example however It still have complex libraries and I need only basic libraries for make a project with CubeMX integrity. LRWAN can not provide that flexibility.

Tesla DeLorean
Guru
Sep 15, 2020 1:19 PM UTC

You'll likely want to refactor the radio SPI code.

The bulk of the initialization in done once. The DIO pins can generate interrupts. The radio link data goes in/out via a FIFO​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..