Skip to main content
Nickelgrass
Senior
Jun 7, 2022 7:29 PM UTC
Solved

Is it possible with CubeIDE to program both cores of the STM32WB55CC? I would like to abuse it as a simple dual core processor without the BLE stack. Just write two bare metal programs, one for each core, and run them. Is this technically possible?

..

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Jun 16, 2022 7:50 AM UTC

Hello,

It's not possible to use CPU2 like this, CPU2 is not accessible.

Best Regards

2 replies

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Jun 16, 2022 7:50 AM UTC

Hello,

It's not possible to use CPU2 like this, CPU2 is not accessible.

Best Regards

Danish1
Lead III
Jul 8, 2022 12:45 PM UTC

On the other hand, I think it is possible to use both processors on STM32WL55 - the LoRa / sub-GHz targeted products.

Whilst I have never done this, I see example applications SubGHz_Phy_PingPong and SubGHz_Phy_PingPong_DualCore (where there is separate code for CM4 and CM0+ cores).

I don't know why ST chose to make the WB55 different in this respect.