Skip to main content
Visitor II
Aug 19, 2024 8:00 AM UTC
Question

Is it possible to scan as a central while establishing a connection to a peripheral?

Hi,

I have an STM32WB board that is working as a central device. I have several peripheral devices, each with an advertising interval of 10 seconds.

As a result, connecting to the devices can take quite some time. Is it possible to scan and receive advertising packets while attempting to connect to a peripheral?

When I try to use the command aci_gap_start_general_discovery_proc after executing aci_gap_create_connection, I receive the error 0x0C.

I also tried using the background scan feature, which can be enabled with aci_hal_write_config_data() (offset parameter 0xC1). However, according to PM0271, section 5.2.1, I'm not entirely sure if this use case aligns with my scenario: "As explained in the previous chapter, in a multi-role scenario, the STM32WB device has the opportunity to advertise, scan, and be connected at the same time with different remote devices."

I don't have a multi-role scenario, so I don't think this feature is appropriate.

If anyone has experience with scanning and connecting simultaneously, could you please share some information?

Thank you!

Best Regards,
Daniel

This topic has been closed for replies.

1 reply

Douglas MILLER
ST Employee
Aug 21, 2024 8:17 PM UTC

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.