Skip to main content
Associate
Jul 26, 2024 4:03 AM UTC
Question

IPCCdataBuffAddr not matching pMb_RefTable (infinite loop)

I read the other forum on this back from 2021, but changing the files didn't do anything. Is there a fix in 2024 now?

 

 

 if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable)
 {
 /*
 * WARNING: If there is a difference between the MAPPING_TABLE placement in memory
 * and the address calculated according to the IPCCDBA option byte,
 * to avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){}
 * Read below, uncomment RCC_OscInitStruct local variable and replace #if 1 by #if 0 if you are sure
 */
 /* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */
#if 1
 /* USER CODE END MBMUXIF_SystemInit_Prevent_OB_Programming */
 Error_Handler();
#else

 

 

This topic has been closed for replies.

2 replies

petera88Author
Associate
Jul 26, 2024 4:49 AM UTC

I'm actually having quite a bit of trouble starting an STM32WL55JC project, and activating SubGHz radio. The generated code doesn't work. How necessary is the MbMux framework? Is there anyway to get a minimal application going? 

None of the dual core example project seem to work.

STTwo-32
ST Technical Moderator
Sep 13, 2024 3:27 PM UTC

Hello @petera88 

If you are looking for a SUBGHZ, I may suggest you take a look at the SubGHz_Phy_PingPong_DualCore example. It should help you.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.