Skip to main content
Associate II
Aug 28, 2023 10:15 AM UTC
Solved

Interface with RF IC

Hi Team,

    Any Transceiver IC support up to 3GHz range in STMicroelectronics? And how to interface with controller.!

 

 

Thanks and Reguad,

Aravind

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Aug 28, 2023 12:59 PM UTC

shure, read the ds.

but for beginner...better look at ready evaluation board, -> ADRV9364-Z7020

 

If you feel a post has answered your question, please click on " Best Answer ".

7 replies

Issamos
Super User
Aug 28, 2023 12:18 PM UTC

Hello @Aravind 

I suggest you to take a look on the STM32WB that works on the frequency of 2.4GHz. But, working on the 3GHz need to have your own concept of technology because classic technologies cover the sub-ghz bands such as LoRa, the 2.4ghz such as Bluetooth and Wi-Fi and the band between 3.1GHz and 9GHz for the UWB technology.

Hope this is helpful for you. If your question is answered please check this answers as a best answer to be diffused.

Best regards.

II

AravindAuthor
Associate II
Aug 28, 2023 12:42 PM UTC

Hi Issamos,

Thanks for your reply,

  Now I want to configure the AD9364 with any other controller ,if it is possible?

Thanks and regards

AScha.3
AScha.3Best answer
Super User
Aug 28, 2023 12:59 PM UTC

shure, read the ds.

but for beginner...better look at ready evaluation board, -> ADRV9364-Z7020

 

If you feel a post has answered your question, please click on " Best Answer ".
Issamos
Super User
Aug 28, 2023 1:25 PM UTC

Hello again @Aravind 

I think this may help you.

Best regards

II

Issamos
Super User
Aug 28, 2023 2:00 PM UTC

Hello again @Aravind

 I suggest you to take a look on this . It should be helpful.

Best regards.

II