Skip to main content
KSaha.11
Visitor II
May 30, 2023 8:49 AM UTC
Question

Inquiry the ST thread rcp product compatible with the matter tool

Hello, 

Recently, I came across an exciting open-source project called ioter, which is based on the Matter thread protocol. github.com/Samsung/ioter

It appears that this project has been verified only with Thread devices based on Nordic nRF52840. However, I would like to know ST thread device is compatible with the tool.

Would you recommend which product is the most compatible. If it would be possible to confirm its compatibility with the Matter project. :thumbs_up: 

This topic has been closed for replies.