Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I purchased a few NUCLEO-WB55RG boards to start testing BLE. I load Github Projects P-NUCLEO-WB55.Nucleo Applications BLE BLE_HeartRate Binary BLE_HeartRate_reference hex on the board to test. Installed st com/en/embedded-software/stblesensor html on my phones (one ios and one android). Connect to a device and it works, screen on the phone shows heart rate data works fine. Unplug the power from the Nucleo board? It never advertises again. I tried all 3 Nucleo boards that I have using the pre-compiled binaries and usually they are difficult to get working, they are not discoverable. But then for some reason the phone detects them and they work. Once. After that they don't work again. Each board I have worked once. Is there a trick to getting the BLE radio to be discoverable? I used the STM32CubeProgrammer FUS to check the FUS infos. On power up, and reading fus info I get:FUS State: FUS_IDLEFUS Status: FUS_NO_ERRORFUS
I am currently working on a project that requires to implement USB audio in and out feature on STM32WB55 for connecting to PC. Is there any reference project that has this driver available? i tried working on FP-AUD-BVLINKWB1 but found that it is only supporting USB audio out and i have no idea how to add audio in into this project. Thank you
Hi I am trying to create SubGHz project using STM32 Cube. When I choose the bl072cz-lrwan1 board, although this is an eval kit for LoRa, and has a PingPong example which uses LoRa and SubGHz, yet I can't find any option for SubGHz or LoRa in the middleware menu. any suggestions what to do ? thanks
Hi there,I have a couple of these boards hooked up to TTN indoor gateway. However after swapping batteries one of them is not joining the network despite using the same files/firmware. Looking at the serial readout, I don't see the usual "Joined = OTAA", just the "MCPS-Confirm" loops, which look the same as the others.Any ideas what could be happening?Kind regards, Oliver
HiWe are using the the ST library calculates LoRa SNR and RSSI by capturing the readings in register "REG_LR_PKTRSSIVALUE" although there is another register called "REG_LR_RSSIVALUE".I failed to figure out the difference in contents of those 2 registers.Any clue ?thanks
Hi I have been trying to activate the callback function for the pushbutton in the SubGHz PingPong example, but with no luck. I am using the BSP_PB_Init() to configure the pushbutton: void BSP_PB_Init(Button_TypeDef Button, ButtonMode_TypeDef ButtonMode) { GPIO_InitTypeDef GPIO_InitStruct; /* Enable the BUTTON Clock */ BUTTONx_GPIO_CLK_ENABLE(Button); __HAL_RCC_SYSCFG_CLK_ENABLE(); if (ButtonMode == BUTTON_MODE_GPIO) { /* Configure Button pin as input */ GPIO_InitStruct.Pin = BUTTON_PIN[Button]; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct); } if (ButtonMode == BUTTON_MODE_EXTI) { /* Configure Button pin as input with External interrupt */ GPIO_InitStruct.Pin = Push
I tried to register an end-node on TTN, but it does not recognize the DevEUI.I watched this video:https://www.youtube.com/watch?v=8KNfrWoa1fw&list=PLnMKNibPkDnHZyJtMRpWSs41CWhPouRwq&index=3error:I have entered the DevEUI here: (I copied the id that is on the board, tried several times but nothing)
Hello,I am trying to build an application on a STM32WLE5JBI6 that could work with confirmed downlinks. I thought that the LoRaMAC handled this but I could not find any mention of it in the documentation or in the code.As anyone already implemented it?I really appreciate any help you can provide.
I want to capture the BLE air packet to parse the BLE connection event by using nRF52840 Dongle and wireshark, but I met a problem.I can capture the air packet normally when the slave device is advertising. But once the connection is established, I can not continue capturing it.I think that it should be related to the BLE security but I don't know how to modify the configuration.If this is the reason, how can I modify the code? If not, what might be the reason.
Dear ST Community, Dear ST Team.For a evaluation of the chip i would like to try over LoRaWAN Communtication to set a LED on and off.Sadly on the tutorial program LoRaWAN_End_Node i get the ERROR: dev_nonce_too_small. The Problem is that on the Documentation from the things Stack i should contact the device’s manufacturer to find out the correct LoRaWAN MAC and PHY versionsI even try out to find a older version of the extension but i dont find any.So im sitting on a dead end and im glad to hear some ideas or information about that topicThanks for your helpRSheetz
Hi, I am currently working on the NUCLEO WB55RG board on a project configured by CubeMX as BLE server. Everything is working correctly on this side. The problem is that I am using 4 boards as server and i would like to send a broadcast message (advertising) from a smartphone that they would all catch at the same time to be able to get a "synchronisation", how can i use my board as client while connected as server so it will catch advertising events?
I'm working on inserting the STM32WB55 into stop mode2 via the tickless idle for the FreeRTOSI saw that the SDK has an example for it: in the BLE_HeartRateFreeRTOS example for the nocleo wb55 I went over the code of the SDK and there was one line which seemed a bit strange to me, in method ReturnTimeElapsed() It seems to me that the if is wrong, and should be: (return_value >= SSRValueOnLastSetup) I didn't run the SDK as is since I had to change some of the code so it will fit the design of our project, But I did had to change the sign of that 'if' statement for it to work. Am I missing here something, has anyone else encountered this?
Hello,I'm using a custom board which has STM32WB55 as the MCU. For the application, requires the MCU in sleep mode. The chosen sleep mode is STOP2. I referred the example project 'PWR_STOP2_RTC' which is available for the p-nucleo board and tried to replicate the same for my custom board. After testing for power consumption, the custom board is taking around 300uA as opposed to ~3uA per datasheet.Can anyone point to me why there is extra consumption, and if there is any more config to be done in the cubeMx or in the code.Thank you in advance.
I am working with the STM32WB15 controller. I have implemented a few custom BLE characteristics and I want to be able to check the value of the characteristics on the server side (not from a read request from a client device). Is there a way to access the current value of a characteristic?
The STM32WL55 Nucleo board comes with the LoraWAN DevEUI, AppKey et al.I assume that this is not the case for STM32WL55CC mcu itself, right? And I have to work out how to write that into each device by myself.// Niclas
Hi,I am trying to commissioning NUCLEO-WB55RG Matter thread end device using chip-tool running on raspberry pi, It fails to commission.Reference Source Code used:Matter beta version for STM32 Github repo: github.com/stm32-hotspot/stm32wb-matter-device-over-thread Setup:1. Matter Thread End DeviceBelow binaries flashed on the STM32 Matter Thread End Device(NUCLEO-WB55).1.1. FUS: "stm32wb-matter-device-over-thread-main\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw.bin" 1.2. BLE Stack: "stm32wb-matter-device-over-thread-main\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_BLE_Thread_ForMatter_fw.bin" 1.3. Application: "stm32wb-matter-device-over-thread-main\Projects\P-NUCLEO-WB55.Nucleo\Applications\Matter\Lighting-App\Lighting-App.bin"2. Border router Raspberry pi(Host) RCP Device(Silabs RCP device)3. Host as a Raspberry pi(chiptool)Also find the Attached logs captured on End device and chiptool running on Raspberry p
I am using the stm32wb boards to learn OpenThread and develop a low power application to read some sensor data. My plan is to use a CoAP message to send the payload, and have been studying the THREAD_SED_Coap_Multicast example in an attempt to learn. When looking at the power consumption of the board, I have been unable to determine the cause of some short spikes in current when in low power. In all the figures shown, I have disabled the SED polling, and the CoAP messages are sent every 30 seconds. I would expect the current to drop to roughly 2.5 uA (as it does) in between messages and stay there, but instead after a transmission, there are exactly 5 small spikes in current, which from their shape I am assuming are radio activity? These are spaced 1 second apart. Then as the sleep cycle goes on, there will be other slightly larger spikes. Here is the consumption over about 80 seconds The tall spikes are the CoAP messages be transmitted This is the shape of the 5 evenly
HiI am building an app where the transmitter has no power constrains, but the receiver needs to run at lowest power.The transmitter (master unit) will be sending pings such that any receiver (slave) near by would respond by sending its ID to the transmitter.Normally, the receiver will be listening (scanning) for the pings from master.I am wondering what is the best practice to reduce the power consumption on the receiver (slave), such that it can be woken up by the transmitter if the receiver is close to the transmitter ? thanks
Hi to all. I have a problem whit USB dongle STM32WB55.With BLE stack and all BLE examples from STM32Cube_FW_WB_V1.16.0 Virtual USB port is working just fine. But when I change to stm32wb5x_Zigbee_FFD_fw and use P-NUCLEO-WB55.USBDongle\Applications\Zigbee\Zigbee_OnOff_Server_Coord Virtual USB port is not working (error code 10). I can turn on and off LED form coordinator (dongle) to router (Nucleo board), and virtual port on Nucleo is working just fine. But virtual port on dongle is not working (erorr code 10).My OS is Win10, I updated Virtual serial port drivers, I changed CDC_DATA_HS_MAX_PACKET_SIZE to 64U but again I have the same problem.Can you please help me.Thanks.
Dear St Community,I'm developing a work at Board Nucleo-WB55RG. I already get the Zigbee communication and USB communication working well on the board, but when I merge them in the same project, I have some problems.My PC identify the USB connection, but in the same project, when I put available the Zigbee on middleware STM32WPAN on the IOC file, I lost this USB connection. So, my PC doesn't identify any more the USB connection after that. Does someone know if there is some conflict between the USB communication and Zigbee on Nucleo-Wb55RG? Or can I solve my problem?
Hello,Can we include the lorawan stack inside the STM32CubeMX?What is the relationship between STM32CubeMX and I-CUBE-LRWAN?Best regardsMichel
After following these examples I am unable to put the device in STOP1/2 low power modes.Can someone please help with implementing low-power modes
Hi, I am using STM32WBA52CG. I am using the STM32 board as BLE_P2P_client, trying to connect my Mobile/ESP32 Server. But the BLE IP address itself not detecting. But, When I am using the STM32 as server, Esp32 can able to communicate with STM. Please advise on how we can create a communication with the external devices when STM32 act as Client. Note: I am using BLE_P2P_client Example. It is reaching to the "analyse_adv_report" function, there i put debug for BLE IP address. It is not detecting the mobile/ESP32 IP. Thanks and Regards, Dinesh Kumar
Hi,Our custom module, built around the STM STM32WLE5CCU6 chipset, has been designed accordingly. However, we have received a new requirement from the customer regarding the EU433 region frequency. Could you please provide us with the application note and reference design necessary to modify our current design to meet the EU433 requirement?Regards,Rahul K V
I need your help with the STM 32wb5mmg. Not sure why power consumption is higher (x2) when VREFBUF is defined as an internal voltage reference. Is this possible because the Vref+ is connected to the VDD?. Appreciated if you could help with this
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.