Skip to main content
Mkuma.7
Associate III
Jan 31, 2023 11:23 AM UTC
Question

If the STM32 is programmed with hex file then it's working fine, If the STM32 is programmed with bin file with the same addresss as hex then it's not behaving same as hex file. Is there any possibility to verify this?

..

This topic has been closed for replies.

4 replies

Javier1
Principal
Jan 31, 2023 12:09 PM UTC

maybe post here both files?

There is a good chance youre not programming both hex and bin files in the same addr

hit me up in https://www.linkedin.com/in/javiermuñoz/
Remi QUINTIN
ST Technical Moderator
Jan 31, 2023 12:09 PM UTC

>it's not behaving same as hex file.

Could you be more explicit?

Hex file format embeds the address where to load the data while the bin file format is only the raw data. For the second case, you need to enter the start address for the flash programming with CubeProgrammer tool.

Remi QUINTIN
ST Technical Moderator
Jan 31, 2023 12:11 PM UTC

What is the CubeProgrammer version you are using?

Could you try with one of the binary file provided in the CubeWB FW package?

Mkuma.7
Mkuma.7Author
Associate III
Feb 7, 2023 8:55 AM UTC

When I flash the hex file, it reboots and Display was functioning(The Display was showing correct value) accordingly, but when I flash the bin file it's not functioning same as hex file.