Skip to main content
MYous.3
Associate
Dec 2, 2021 6:06 PM UTC
Question

IEEE 802.15.4 Encryption

Hey All,

I want to add encryption to the existing STM32WB55 MAC 802.15.4 ​FFD/RFD examples.

How could i ensure encryption and integrety of my data. As i consulted the IEEE 802.15.4 standard​, I can use the ENC-MIC-128 for both encryption and integrity, by setting the 'security enabled' field and setting the Auxiliary Security Header 'ASH' fields accordingly.

My question is how exactly to do that, because not all PIB attributes concerning the ​ASH are available on the ST implementation for mac_802.15.4 ?

Also there is the concept for the Security Table that stores different Keys, i couldn't find any related fields or PIBs.

Please can you provide me with how to add security​ to existing STM32WB55 examples.

This topic has been closed for replies.

2 replies

Remi QUINTIN
ST Technical Moderator
Dec 10, 2021 9:09 AM UTC

Encryption is not supported by our IEEE 802.15.4 MAC STM32WB solution.

So, if you want to authenticate or cypher your data, you have to encrypt the payload provided to the MAC layer. (ie : It is up to the Mac client layer - NWK layer -to handle cyphering process as it is implemented with ZB).

There is no plan to provide mac encryption for STM32WB.

MYous.3
MYous.3Author
Associate
Dec 10, 2021 1:07 PM UTC

It is a big disappointment, but it is not exactly surprising.