Skip to main content
BMart.2
Associate III
Jul 15, 2020 4:34 PM UTC
Question

I2C Error Trapping

0693W000001sxN6QAI.pngI am using the STM32WB in master mode, polling a single LSM303AGR accelerometer. Using the HAL transmit routine as follows:

if(hi2c1.State == HAL_I2C_STATE_READY)

 {

  /* Now send the device address and register to be read with 1 sec delay max*/

  while(HAL_I2C_Master_Transmit(&hi2c1, DEVICE_ADDR, i2cbuffer, 1, 1000) != HAL_OK)

  {

   /* Error_Handler() function is called when Timeout error occurs.

     When Acknowledge failure occurs (Slave doesn't acknowledge its address)

     Master restarts communication */

   if (HAL_I2C_GetError(&hi2c1) != HAL_I2C_ERROR_AF)

   {

    errorcount = 20;

    Error_Handler();

   }

  }

   

  /* Now get the return byte of the register in i2cbuffer[0, 1] with 1 sec delay max*/

  while(HAL_I2C_Master_Receive(&hi2c1, DEVICE_ADDR, i2cbuffer, 2, 1000) != HAL_OK)

  {

   /* Error_Handler() function is called when Timeout error occurs.

     When Acknowledge failure occurs (Slave doesn't acknowledge it's address)

     Master restarts communication */

   if (HAL_I2C_GetError(&hi2c1) != HAL_I2C_ERROR_AF)

   {

    errorcount = 21;

    Error_Handler();

   }

  }

  

  tmp = i2cbuffer[1];

  tmp = (tmp<<8) & 0x0000ff00;

  tmp = (tmp | i2cbuffer[0]) & 0x0000ffff;

   

  rtnval = (int16_t)tmp;

 }

The last two variables in the debug window are obtained as follows at the start of the Error_Handler() routine:

uint32_t itflags  = READ_REG(hi2c1.Instance->ISR);

 uint32_t itsources = READ_REG(hi2c1.Instance->CR1);

Not interrupt, just polling. Every so often, it jumps to the Error_Handler() routine which just toggles an LED in a while(1) loop indefinitely. I am trying to determine the cause of this error.

Attached is a picture of the debugger screen showing the i2c instance and all relevant variables. From this picture, can anyone help me determine the cause of the error? It's taking 2 days of runtime to catch this so any help would be appreciated.

Thanks

This topic has been closed for replies.

1 reply

TDK
Jul 15, 2020 8:51 PM UTC

Duplicate of:

https://community.st.com/s/question/0D53W00000Cgz7WSAR/i2c-error-trapping

Please don't post the same problem multiple times.

"If you feel a post has answered your question, please click ""Accept as Solution""."