Skip to main content
SSing.3
Associate
May 13, 2020 6:12 PM UTC
Question

I want to use two B-L072Z-LRWAN, one as an end node and the other as a gateway. I am all set with the end node but is it possible to set B-L072Z-LRWAN as a gateway between the server and the end node.

..

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
May 13, 2020 6:22 PM UTC

The radio can receive the signals, you'd have to own the task ​of writing the gateway functionality.

​

It is not well suited to dealing with multiple nodes transmitting at random times, and on top of each other.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
May 13, 2020 7:18 PM UTC

A pair of B-L072Z-LRWAN can be used in a point-to-point mode, more could broadcast one-to-many.

For a gateway class device look at https://www.st.com/en/evaluation-tools/p-nucleo-lrwan3.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SSing.3
SSing.3Author
Associate
May 13, 2020 8:56 PM UTC

Can I have two  B-L072Z-LRWAN talking to each other?

Tesla DeLorean
Guru
May 13, 2020 9:23 PM UTC

Yes, like I said point-to-point

The ping-pong example alternates, but you could just as easily have a committed transmitter, and a committed receiver, and send GPS coordinates and temperature measurements, for example

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..