I want to add jason parser using UART in my stm32 code. I used json.c and json.h files in the code. I can get the output in the compile time. But when I use run time I am not getting the output logically. Kindly help me.
- 0 replies
- 1906 views
callback:
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
uint8_t i;
if (huart->Instance == USART1) //current UART
{
if (Rx_indx==250) {for (i=0;i<100;i++) Rx_Buffer[i]=0;} //clear Rx_Buffer before receiving new data
if (Rx_data[0]!=13) //if received data different from ascii 13 (enter)
{
Rx_Buffer[Rx_indx++]=Rx_data[0]; //add data to Rx_Buffer
}
else //if received data = 13
{
Rx_indx=0;
Transfer_cplt=1;//transfer complete, data is ready to read
}
HAL_UART_Receive_IT(&huart1, Rx_data, 1); //activate UART receive interrupt every time
}
}
main.c
HAL_UART_Receive_IT(&huart1, Rx_data, 1); //activate uart rx interrupt avery time receiving 1 byte
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
i = 0;
if (Transfer_cplt != 0)
{
//HAL_UART_Transmit(&huart1, "t", 1, 1000);
for(int a=0;a<13;a++)
{
HAL_UART_Transmit(&huart1, Rx_Buffer, strlen(Rx_Buffer), 1000);
JSONObject *json = parseJSON(Rx_Buffer);
//HAL_UART_Receive(&huart1, json, strlen(json), 1000);
printf(" %s : %s\r\n", json->pairs[a].key, json->pairs[a].value->stringValue);
Transfer_cplt=0; //reset transfer_complete variable
HAL_Delay(500);
i++;
}
i = 1;
}