Skip to main content
Visitor II
Aug 8, 2025 8:35 AM UTC
Solved

I-NUCLEO-LRWAN1 Still Supported?

Hi all,

As part of a uni project we are developing a LoRaWAN Weather station project.

We have free access (the team is operated on a limited budget) to a I-NUCLEO-LRWAN1 board. This appears to be a very good option as the board has all the integrated sensors required, and is compatible with Australian frequency.

How good is the support and integration with current development tools, I see the suggested board on the datasheet is still currently sold (NUCLEO-L053R8). 

Does anyone have experience with this board, or can point in the direction of something more suitable?

Thanks

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 8, 2025 8:46 AM UTC

Hello @sr71brd and welcome to the ST Community.

The I-NUCLEO-LRWAN1 is an obsolete product (as you can see on the product webpage). If you are looking for a product to establish a LoRaWAN connection based on the STM32, i suggest you use the STM32WL (This series provides a portfolio of System-On-Chip solutions integrating both a low-power microcontroller and a long-range, energy-efficient sub-GHz radio (that support the LoRa transmission for LoRaWAN) on the same chip.). As a evaluation board, you may use the NUCLEO-WL55JC without a need to a host board (all in the same SOC).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 8, 2025 8:46 AM UTC

Hello @sr71brd and welcome to the ST Community.

The I-NUCLEO-LRWAN1 is an obsolete product (as you can see on the product webpage). If you are looking for a product to establish a LoRaWAN connection based on the STM32, i suggest you use the STM32WL (This series provides a portfolio of System-On-Chip solutions integrating both a low-power microcontroller and a long-range, energy-efficient sub-GHz radio (that support the LoRa transmission for LoRaWAN) on the same chip.). As a evaluation board, you may use the NUCLEO-WL55JC without a need to a host board (all in the same SOC).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Aug 8, 2025 9:10 AM UTC

As @STTwo-32 said, the I-Nucleo-LRWAN1 is obsolete:

AndrewNeil_0-1754643855716.png

It has been for a long time and, to be frank, the support was never great in the first place.

If you want a challenge, the schematics of the USI module can be found;  it just uses a standard STM32 and Semtech chips - so you could (in principle) write your own code...

 

Apart from the WL SoCs already mentioned, there is also the B-L072Z-LRWAN1 - which is still marked as Active:

https://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.