Skip to main content
bdaniel7
Associate
Sep 20, 2018 2:00 PM UTC
Question

I-NUCLEO-LRWAN1 compatible boards?

Hi,

I have two boards that I would like to use with the I-NUCLEO-LRWAN1 expansion board:

NUCLEO-F411RE and NUCLEO-L152RE.

Is any of them compatible with I-NUCLEO-LRWAN1?

Thanks.

    This topic has been closed for replies.

    4 replies

    ST Technical Moderator
    Sep 20, 2018 2:57 PM UTC

    Hello @DB.7lendea​ ,

    Yes, these boards are compatible with  I-NUCLEO-LRWAN1.

    You can check the compatible products and softwares on the board page:

    https://www.st.com/en/evaluation-tools/nucleo-f411re.html

    https://www.st.com/en/evaluation-tools/nucleo-l152re.html

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Tesla DeLorean
    Guru
    Sep 20, 2018 3:14 PM UTC

    You're talking through the USART on D0/D1 of the shield, I don't think NUCLEO-64 boards are ideal for that as you have some clashing with the VCP, but you should be able to resolve with SB (solder bridges) changes.

    The NUCLEO-144 or DISCO boards with shield would be arguably better choices.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bdaniel7
    bdaniel7Author
    Associate
    Sep 21, 2018 7:17 AM UTC

    Ok, noted.

    Thanks.

    bdaniel7
    bdaniel7Author
    Associate
    Sep 21, 2018 1:50 PM UTC

    Hmm,

    I see in the technical documentation for the I-CUBE-LRWAN software, only the following boards are supported:

    NUCLEO-L053R8

    NUCLEO-L073RZ

    NUCLEO-L152RE

    NUCLEO-L476RG

    Do I need to make some changes in the software to be able to use the F411RE board?