Skip to main content
yjae
Associate II
Aug 18, 2018 3:45 AM UTC
Question

I'm going to run a ping-pong example with two p-nucleo-lrwan1.

I'm going to run a ping-pong example with two p-nucleo-lrwan1. How do I separate the master from the slave? Terminal uses 'tera Term'.

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Aug 18, 2018 5:05 AM UTC

    The first unit running becomes the master, and a secondary unit receiving the message switches to slave mode. There can be some meta-stability and you can likely alter the state by resetting.

    The basic test here is that they transmit back and forth and see each other.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    yjae
    yjaeAuthor
    Associate II
    Aug 18, 2018 10:18 AM UTC

    Thank you. I want to check if it works like ping-pong exemple in the p-nucleo-lrwan1 manual. However, the terminal does not show the 'it's 0:0:3:930 WU@ 0:0:4:930'.Is this right?