I keep getting an error with some of the example projects where files cannot be found when they do exist in the folder structure for the project and are pointed to in Atollic's (9.3) directory build reference.
Specifically, I am trying to compile the STM32WB Dongle Thread General CoAP example.
Although this isn't a problem specific to STM32 but more with the IDE, I was hoping somebody might have a hint on how to solve the issue. Also, all of the files exist within the scope of the workspace.
Error:
Info: Internal Builder is used for build
arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32WBxx_HAL_Driver\Src\stm32wbxx_hal_cortex.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DCORE_CM4 -DUSE_HAL_DRIVER -DUSE_STM32WBXX_USB_DONGLE -DTHREAD_WB -DSTM32WB55xx -DST_OT_DEBUG -DOPENTHREAD_CONFIG_FILE=<openthread_api_config_ftd.h> -I../../../../../../../../Drivers/STM32WBxx_HAL_Driver/Inc -I../../../../../../../../Drivers/CMSIS/Include -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32WBxx/Include -I../../../../../../../../Drivers/BSP/P-NUCLEO-WB55.USBDongle/ -I../../../Core/Inc -I../../../STM32_WPAN/App -I../../../STM32_WPAN/Target -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/stack/include -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/stack/include/openthread -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/core/openthread_api -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread -I../../../../../../../../Middlewares/ST/STM32_WPAN/utilities -I../../../../../../../../Utilities/lpm/tiny_lpm -I../../../../../../../../Utilities/sequencer -I../../../../../../../../Middlewares/ST/STM32_WPAN -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/tl -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/shci -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/vcp -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Drivers\STM32WBxx_HAL_Driver\stm32wbxx_hal_cortex.o
arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_WPAN\thread\openthread\core\openthread_api\diag.c -mthumb -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -std=gnu11 -DCORE_CM4 -DUSE_HAL_DRIVER -DUSE_STM32WBXX_USB_DONGLE -DTHREAD_WB -DSTM32WB55xx -DST_OT_DEBUG -DOPENTHREAD_CONFIG_FILE=<openthread_api_config_ftd.h> -I../../../../../../../../Drivers/STM32WBxx_HAL_Driver/Inc -I../../../../../../../../Drivers/CMSIS/Include -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32WBxx/Include -I../../../../../../../../Drivers/BSP/P-NUCLEO-WB55.USBDongle/ -I../../../Core/Inc -I../../../STM32_WPAN/App -I../../../STM32_WPAN/Target -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/stack/include -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/stack/include/openthread -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread/core/openthread_api -I../../../../../../../../Middlewares/ST/STM32_WPAN/thread/openthread -I../../../../../../../../Middlewares/ST/STM32_WPAN/utilities -I../../../../../../../../Utilities/lpm/tiny_lpm -I../../../../../../../../Utilities/sequencer -I../../../../../../../../Middlewares/ST/STM32_WPAN -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/tl -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/shci -I../../../../../../../../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/vcp -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Inc -I../../../../../../../../Middlewares/ST/STM32_USB_Device_Library/Core/Inc -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -specs=nano.specs -o Middlewares\STM32_WPAN\thread\openthread\core\openthread_api\diag.o
..\..\..\..\..\..\..\..\Middlewares\ST\STM32_WPAN\thread\openthread\core\openthread_api\diag.c:25:42: fatal error: stm32wbxx_core_interface_def.h: No such file or directory
#include "stm32wbxx_core_interface_def.h"
EDIT:
I swapped out all relative paths to include paths, thinking that may have messed something up. Still getting the same error.