Question
I have two different STM32WB55 Nucleo boards in a state where the debugger cannot connect to the target. Is there an errata I'm missing?
I am using the ST32CubeIDE and the imported HeartRate project from the STM32CubeWB package. For both boards the project compiles and is loaded into the board, and then the boards just stop working during debugging. I am not probing the boards or touching them in any way. This is the oddest thing I've ever seen. Has anyone else experienced this?