Skip to main content
scora.1
Visitor II
Mar 20, 2023 7:15 AM UTC
Question

I have designed a STM32WL55JC2 board with reference to en.MB1389-WL55JC-lowband-D04_Schematic and got it manufactured. Now When i try to program the chip with STM32CubeIde version 1.11.2, the following error occurs.

Log output file:  C:\Users\ASHSIR\AppData\Local\Temp\STM32CubeProgrammer_a10808.log

ST-Link Server is running on port : 7184

ST-LINK SN : 3A2C0A0011145243574D4E00

ST-LINK FW : V2J37S7

Board    : --

Voltage   : 3.18V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x497

Revision ID : Rev Y

Device name : STM32WLxx

Flash size : 256 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xC4

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a10808.srec

 File     : ST-LINK_GDB_server_a10808.srec

 Size     : 36.83 KB 

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 18]

Error: failed to erase memory

Error: failed to erase memory

Encountered Error when opening C:\ST\STM32CubeIDE_1.10.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.500.202209151145\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

For this problem, I need to chip erase with BOOT0 pin high using stm32Cubeprogrammer every time before i upload the program. Some time debugging also doesn't work.

This topic has been closed for replies.