Skip to main content
clf88
Associate
Nov 6, 2018 4:30 PM UTC
Solved

I-CUBE-LRWAN ping pong example

Hi all,

I am modifing the Ping Pong example of the I-CUBE-LRWAN; I am working with a L073RZ nucleo board and the SX1272MB2xAS LoRa shield.

I was performing some experiment (changing spreading factor, code rate, bandwidth) and the example with SF = 11 and SF = 12 doesn't work on the receiver side.

I did not change anything in the example provided by ST: only the spreading factor, which work for SF = 7, 8, 9 and 10.

Someone with the same issue?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 6, 2018 4:34 PM UTC

>>SF = 12 doesn't work on the receiver side

Watch the timeout vs tx time, the timeout will abort an active/on-going reception

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 6, 2018 4:34 PM UTC

>>SF = 12 doesn't work on the receiver side

Watch the timeout vs tx time, the timeout will abort an active/on-going reception

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
clf88
clf88Author
Associate
Nov 6, 2018 4:46 PM UTC

So obvious! The timeout at rx was 1 second...

Thank you so much!

AChaa.15
Associate
Jun 19, 2019 9:55 AM UTC

Hello !

I'm working in the same program of the ping pong with SF =10 and the program works only in RX_timeout and TX_timeout

is there any solution please ?

thank you