Skip to main content
SYun.2
Associate II
Jul 30, 2021 6:47 AM UTC
Question

I-CUBE-LRWAN AT_SLAVE example AT_DevEUI_set

Hello

I am experiencing two problems.

My development environment is STM32L072CZ-LRWAN1.

You are now using a combination of END_NODE and AT_SLAVE examples.

I'll sort out my problems.

The first is that 'SET' values are not operated through features such as AT+DEVEUI, AT+APPEUI, etc.

#define STATIC_DEVICE_EUI 0

Modified to above define to change settings.

but

AT+DEUI=11:22:33:44:55:66:77:88

AT_ERROR

As shown above, only errors continue to occur and do not change.

AT+DEUI=?

AT+DEUI?

The above 2 functions operate normally.

I will attach the serial output as a picture

0693W00000D1475QAB.jpg 

The second is that once the MCU is reset, it stops working.

0693W00000D147UQAR.jpg 

I'm currently using LPUART1.

Please advise how to solve this problem.

This topic has been closed for replies.

1 reply

SYun.2
SYun.2Author
Associate II
Aug 27, 2021 12:48 AM UTC

I found a solution for myself.

I'm posting it because I think there are people who are having the same problem as me.

Please check if the NVIC setting is not wrong.

In my case, I believe that the interrupts between SPI and GPIO collided during the interrupts of the pins that are commonly used with the SPI pins during the GPIO setup process.