Skip to main content
Visitor II
Nov 25, 2024 3:48 AM UTC
Question

I-CUBE-LRWAN

Hi

I'm working on a project where I have to take the humidity and temperature measures of the soil, and send them to a LoraWAN getaway. The problem is that I have to use the STM32L010F4P6 microcontroller and the RF module LAMBDA62C-9S. My question is if the i-cube-lrwan software expansion can help me to load the LoRaWAN firmware in the microcontroller and use the Lambda module to do this. 

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Nov 25, 2024 4:51 AM UTC

Perhaps, but 16KB FLASH, and 2KB RAM, might prove a tad challenging.

Try building something, see what the foot-print actually looks like. Look at a generic Semtech library build for the SX1262, or something lighter weight.

The Murata module has an L072 w/192KB FLASH

Perhaps converse with the engineer who made the part choices..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..