Skip to main content
BMart.2
Associate III
Apr 11, 2020 6:47 PM UTC
Question

I am using the CubeMX example UART_Hyperterminal_IT.ioc file to generate a IAR project to connect a P-Nucleo board to a PC running Hyperterminal. Is there code to add after you generate the project as i can't seem to get it to work? Any help apprecia

..

This topic has been closed for replies.

1 reply

Le Corre Pierre
ST Employee
Apr 14, 2020 1:09 PM UTC

​Hello @BMart.2​ ,

Can you indicate us the version of STM32CubeMX and STM32CubeWB you are using?

In addition, this example comes with the IAR project ready to run: Projects\P-NUCLEO-WB55.Nucleo\Examples\UART\UART_HyperTerminal_IT\EWARM

Did you try it before generating the project with STM32CubeMX?

A more precise description of what you observe would help solve your problem.

BR.

Pierre.