Skip to main content
gasda.1
Associate
May 17, 2020 4:37 PM UTC
Solved

HSEM HAL strange behavior

Hi,

I'm playing around HSEM module and i noticed strange behavior. Why calling:

HAL_HSEM_FastTake(HSEM_ID_0);

or

HAL_HSEM_Take(HSEM_ID_0, 0);

lock all semaphores at once instead of just locking single semaphore specified by a macro using 0 as processid?

Then calling release will unlock only the one specified macro and we end up with 31 semaphores locked unintentionally.

This topic has been closed for replies.
TDK
TDKBest answer
May 23, 2020 2:37 PM UTC

Reading the RLR (read lock register), which you are doing by examining the value in peripheral mode, will lock the semaphore. Disable the RLR registers from being viewed.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
May 18, 2020 1:47 AM UTC

Why do you think it's locking all 32 semaphores?

"If you feel a post has answered your question, please click ""Accept as Solution""."
gasda.1
gasda.1Author
Associate
May 23, 2020 10:56 AM UTC

Because i've check it with debugger

This is state before calling HAL_HSEM_FastTake:

0693W000001pKq8QAE.png

and this is after:

0693W000001pKqDQAU.png

As you can see all semaphores has been locked by main cpu

TDK
TDKBest answer
May 23, 2020 2:37 PM UTC

Reading the RLR (read lock register), which you are doing by examining the value in peripheral mode, will lock the semaphore. Disable the RLR registers from being viewed.

"If you feel a post has answered your question, please click ""Accept as Solution""."
gasda.1
gasda.1Author
Associate
May 23, 2020 3:23 PM UTC

Oh you are defenitely right, viewing in peripheral mode does lock every semaphore. Thanks for clarification!