Skip to main content
lastMcu
Associate II
Jul 17, 2024 1:28 AM UTC
Solved

HSE with PLL for STM32WB at 64MHZ

There doesn't seem to be any project in the whole STM32CubeWB package that uses the HSE with PLL. At least I couldn't find any with a .IOC file. Most samples in the package use the MSI clock, except, of course, for the wireless projects that use HSE for better accuracy. But in all those projects that use the HSE, they use the clock directly, not through the PLL, and then they clock the main CPU at 32 MHz, not at 64 MHz.

 

Of course it is possible to modify the configuration to use the HSE with the PLL. But it is rather strange that with all the projects in the package, everyone that do use the HSE, doesn't use the PLL and chooses to configure the CPU at a lower frequency. To be honest, it makes one suspicious that it could be a problem and it might not work reliably if one try to use the HSE with the PLL.

 

Anybody has any actual experience with a wireless project using the HSE and clocking the CPU at 64 MHz through the PLL?

 

Thanks

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 24, 2024 4:25 AM UTC

I can't see any potential problem in running the STM32WB with a HSE PLL frequency of 64 MHz. It should work fine.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Remy ISSALYS
ST Technical Moderator
Jul 19, 2024 2:57 PM UTC

Hello,

You can find BLE_HeartRate_PLL example in STM32CubeWB package witch used the PLL as system clock.

Best Regards

lastMcu
lastMcuAuthor
Associate II
Jul 20, 2024 4:04 AM UTC

@Remy ISSALYS wrote:

You can find BLE_HeartRate_PLL example in STM32CubeWB package witch used the PLL as system clock.

Are you sure it uses the PLL as system clock? I can see that the PLL is configured to use HSE. But I don't see that the PLL is connected to the system clock:

 

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 ...
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

 

As you can see, HSE is connected to the system clock directly, not through the PLL. Also, the configured flash latency would be too low for a 64 MHz clock.

STTwo-32
ST Technical Moderator
Jul 23, 2024 2:06 PM UTC
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.