Skip to main content
ledi001
Associate III
Jan 8, 2025 3:48 PM UTC
Solved

How to use LSI instead of LSE with STM32WBA55

Hi,

I use the example “BLE_p2pServer_ota” with NUCLEO-WBA55 as a template for a project.
For space reasons and to save costs, I would like to use the internal oscillator LSI1 (32,000kHz) instead of the external 32,768 chrystal LSE. After switching to LSI1 with CubeMX, the advertising works, but a connection can no longer be established. Which workaround is required to use the LSI?

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jan 8, 2025 6:00 PM UTC

Hello @ledi001 

Do you mean you have replaced LSE with LSI1 in all peripherals that uses LSE. If so, The LSI1 must not be used for the 2.4 GHz RADIO sleep timer.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jan 8, 2025 6:00 PM UTC

Hello @ledi001 

Do you mean you have replaced LSE with LSI1 in all peripherals that uses LSE. If so, The LSI1 must not be used for the 2.4 GHz RADIO sleep timer.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ledi001
ledi001Author
Associate III
Jan 8, 2025 6:16 PM UTC

Hello @STTwo-32 

Thank you for your reply. Does this mean that there is no other option than to use the LSE in this case?

Tesla DeLorean
Guru
Jan 8, 2025 6:47 PM UTC

Only the LSE lives in the Backup Domain wrt to power, on the STM32WB55 and frankly most of the STM32 families

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..