Skip to main content
MPian.1
Associate II
Jun 1, 2021 12:26 PM UTC
Solved

How to turn off and restart the BLE core in STM32WB50

I'm working with a STM32WB50. To save energy i have to turn off BLE when i don't need it and turn on when i need it.

This topic has been closed for replies.
Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Jul 19, 2021 2:40 PM UTC

You do not need to start and stop the BLE core. If you do not send any commends to the BLE core, the BLE core remains in low power STOP2 mode.

So, at the end of the current command being processed by the BLE stack, The M0+ core enters STOP2 mode.

If you want the BLE core not to respond to any connection, just close them.

Otherwise during no RF activity periods, the M0+core is in STOP2 mode, which is consuming very few power, around 2uA.

1 reply

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Jul 19, 2021 2:40 PM UTC

You do not need to start and stop the BLE core. If you do not send any commends to the BLE core, the BLE core remains in low power STOP2 mode.

So, at the end of the current command being processed by the BLE stack, The M0+ core enters STOP2 mode.

If you want the BLE core not to respond to any connection, just close them.

Otherwise during no RF activity periods, the M0+core is in STOP2 mode, which is consuming very few power, around 2uA.