Skip to main content
Associate
Apr 7, 2025 8:51 AM UTC
Question

How to solve the ADC problem when exiting stop mode in STM32WB5

I'm using an STM32WB5MMG module.
I was facing a problem with AD not working properly when exiting from stop2 mode.

HAL_ADC_PollForConversion()

returns a value other than HAL_OK
And,

HAL_ADC_GetValue(&hadc1)

returns only 0.

I have confirmed the same problem in the following post, but it remained unresolved, so I would like to know how to resolve it.
https://community.st.com/t5/stm32-mcus-wireless/how-to-get-adc-to-work-after-stop0-mode-stm32wb5/td-p/95710

Similar to this post
Before entering STOP2 mode, tried to do

HAL_ADC_DeInit(&hadc1);

and after exiting from STOP2 mode, tried to do

MX_ADC1_Init()

But, The process in this function below had error.

if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }


Is there any approach I should try?

This topic has been closed for replies.

3 replies

Yuki_IAuthor
Associate
May 1, 2025 1:50 AM UTC

Hi,
any information on this topic?

STTwo-32
ST Technical Moderator
May 5, 2025 3:10 PM UTC

Hello @Yuki_I 

Could you please share the code that you used to show the ADC is working fine before STOP2 mode and it gets an error after.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Yuki_IAuthor
Associate
May 8, 2025 1:31 AM UTC

Hello, @STTwo-32 

The code I am trying is below.
I am using cubeMX V6.12 and CubeFW_WB V.1.20 for code generation.
in main.c

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */
 MX_APPE_Config();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* Configure the peripherals common clocks */
 PeriphCommonClock_Config();

 /* IPCC initialisation */
 MX_IPCC_Init();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RTC_Init();
 MX_TIM16_Init();
 MX_ADC1_Init();
 MX_RF_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADC_DeInit(&hadc1);
 /* USER CODE END 2 */

 /* Init code for STM32_WPAN */
 MX_APPE_Init();

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 
 
 HAL_TIM_Base_Start_IT(&htim16);

 while (1)
 {
 /* USER CODE END WHILE */
 
 MX_APPE_Process();

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
 uint16_t ADCdata12bit = 0;

 //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
 if (HAL_ADC_Start(&hadc1) != HAL_OK)
 {
 /* ADC conversion start error */
 
 //Error_Handler();
 }
 /* Wait for ADC conversion completed */
 if (HAL_ADC_PollForConversion(&hadc1, 10) != HAL_OK)
 {
 /* End Of Conversion flag not set on time */
 //Error_Handler();
 }
 
 ADCdata12bit = HAL_ADC_GetValue(&hadc1);
 
 if(HAL_ADC_Stop(&hadc1) != HAL_OK)
 {
 //Error_Handler();
 }

 //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
}

 in app_entry.c

void MX_APPE_Init(void)
{
 System_Init(); /**< System initialization */

 SystemPower_Config(); /**< Configure the system Power Mode */

 HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

/* USER CODE BEGIN APPE_Init_1 */
 APPD_Init();
 UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
/* USER CODE END APPE_Init_1 */
 appe_Tl_Init();	/* Initialize all transport layers */

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

 return;
}

 in app_ble.c

void APP_BLE_Init(void)
{

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~

/**
 * Initialize Ble Transport Layer
 */
 Ble_Tl_Init();

 /**
 * Do not allow standby in the application
 */
 UTIL_LPM_SetOffMode(1 << CFG_LPM_APP_BLE, UTIL_LPM_DISABLE);

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

 /**
 * Start to Advertise to be connected by a Client
 */
 Adv_Request(APP_BLE_LP_ADV);

}

SVCCTL_UserEvtFlowStatus_t SVCCTL_App_Notification(void *p_Pckt)
{

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

switch (p_event_pckt->evt)
 {
 case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
 {
 p_connection_complete_event = (hci_le_connection_complete_event_rp0 *) p_meta_evt->data;
 /**
 * The connection is done, there is no need anymore to schedule the LP ADV
 */

 APP_DBG_MSG(">>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x%x\n", p_connection_complete_event->Connection_Handle);
 APP_DBG_MSG(" - Connection established with Central: @:%02x:%02x:%02x:%02x:%02x:%02x\n",
 p_connection_complete_event->Peer_Address[5],
 p_connection_complete_event->Peer_Address[4],
 p_connection_complete_event->Peer_Address[3],
 p_connection_complete_event->Peer_Address[2],
 p_connection_complete_event->Peer_Address[1],
 p_connection_complete_event->Peer_Address[0]);
 APP_DBG_MSG(" - Connection Interval: %.2f ms\n - Connection latency: %d\n - Supervision Timeout: %d ms\n\r",
 p_connection_complete_event->Conn_Interval*1.25,
 p_connection_complete_event->Conn_Latency,
 p_connection_complete_event->Supervision_Timeout*10
 );

 if (BleApplicationContext.Device_Connection_Status == APP_BLE_LP_CONNECTING)
 {
 /* Connection as client */
 BleApplicationContext.Device_Connection_Status = APP_BLE_CONNECTED_CLIENT;
 }
 else
 {
 /* Connection as server */
 BleApplicationContext.Device_Connection_Status = APP_BLE_CONNECTED_SERVER;
 }
 BleApplicationContext.BleApplicationContext_legacy.connectionHandle = p_connection_complete_event->Connection_Handle;
 /**
 * SPECIFIC to Custom Template APP
 */
 HandleNotification.Custom_Evt_Opcode = CUSTOM_CONN_HANDLE_EVT;
 HandleNotification.ConnectionHandle = BleApplicationContext.BleApplicationContext_legacy.connectionHandle;
 Custom_APP_Notification(&HandleNotification);
 /* USER CODE BEGIN HCI_EVT_LE_CONN_COMPLETE */
 //BLEConnectionStatus = BleApplicationContext.Device_Connection_Status;
 UTIL_LPM_SetStopMode(1 << CFG_LPM_APP_BLE, UTIL_LPM_DISABLE);
 UTIL_LPM_SetStopMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
 //To make sure that the device is not in stop mode when connected.
 APP_BLE_Reconnection_Status = 1;

 /* USER CODE END HCI_EVT_LE_CONN_COMPLETE */
 break; /* HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE */
 }
 //~~~~~~~~~~~~~~~~~~~~~~~~~~

}

On this code, in app_conf.h

#define CFG_LPM_SUPPORTED 0
the ADC will work correctly after BLE connection,
#define CFG_LPM_SUPPORTED 1
in main.c
HAL_ADC_PollForConversion(&hadc1, 10)
an error is generated.