Skip to main content
Eshin.1
Visitor II
Apr 9, 2020 11:02 AM UTC
Question

How to set WB55 with MBedOS

Dear.

​

I use WB55 with MBed OS.

​

I needed to receive huge file(over 1M) from Android and

​

send to Another Device by SPI interface.

​

It sometimes work well. but mostly I met hardFault by monitoring Serial.

Android App setting

- requestMTU :241

Connection Interval : CONNECTION_PRIORITY_HIGH 

(ConnectionInterval: 12/ConnectionLatency: 0/ConnectionSupervisionTimeout: 500)

Data Send interval : 50ms(after confirmed send Data)

Write Type: Write_NO_RESPONSE

Data SIze : over 1M

WB55 setting :

 "cordio.rx-acl-buffer-size":245,

      "cordio.max-att-writes":1,

      "cordio.desired-att-mtu": 241

MemoryPool /Queue size 16

CODE Structure :

Data received(BLE) - MemoryPool alloc - Queue -> Check Queue Evevt(Another Thread) - Data Send(SPI) - Free MemoryPool

Situation :

Board Stuck after receiving some Data. and displayed HARD_FAULT after few moment.

++ MbedOS Fault Handler ++

FaultType: HardFault

Context:

R0  : 20000508

R1  : 00000000

R2  : E7D85466

R3  : 0000008C

R4  : 00000001

R5  : 20004F58

R6  : 006200F0

R7  : 200053E0

R8  : 00000000

R9  : 00000000

R10 : 00000000

R11 : 00000000

R12 : FFFFFFFF

SP  : 2002FFC0

LR  : 0802311D

PC  : E7D85466

xPSR : 40000035

PSP : 20004950

MSP : 2002FFA0

CPUID: 410FC241

HFSR : 40000000

MMFSR: 00000001

BFSR : 00000000

                                                                                               UFSR : 00000000

DFSR : 00000000

AFSR : 00000000

Mode : Handler

Priv : Privileged

Stack: MSP

-- MbedOS Fault Handler --

                                                                                                                                                                                                               ++ MbedOS Error Info ++

Error Status: 0x80FF013D Code: 317 Module: 255

Error Message: Fault exception

Location: 0xE7D85466

Error Value: 0x200030D8

Current Thread: rtx_idle <handler> Id: 0x20004644 Entry: 0x801D475 StackSize: 0x300 StackMem: 0x200046D0 SP: 0x2002FFC0

For more info, visit: https://mbed.com/s/error?error=0x80FF013D&tgt=NUCLEO_WB55RG

                                                                                                                                                                                                                                                       -- MbedOS Error Info --

plz help me to solve this problem.

thanks.

​

This topic has been closed for replies.