Skip to main content
GMaud
Associate II
Sep 24, 2020 1:02 PM UTC
Solved

How to set up CubeMX for STM32WLE5JCIx or even STM32WLE5CCUx ?

I have CubeMX installed and when selecting SMT32WL family I get three BGA devices to select, but when I want to start a project based on these,

I get the error: "STM32CubeMX cannot load this Mcu"

I have CubeMX 6.0.1 and all packages installed.

I would also prefer to have the QFN package in the tool, because that is the device I want to use on my boards.

This topic has been closed for replies.
Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Sep 24, 2020 1:08 PM UTC

​Though you can select a WL device, you cannot get any sw supported for it via CubeMX  as it is not officially delivered as of today.

1 reply

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Sep 24, 2020 1:08 PM UTC

​Though you can select a WL device, you cannot get any sw supported for it via CubeMX  as it is not officially delivered as of today.